REGEN.VOLTSHIGH
Description
This parameter returns the DC bus voltage at which the regen circuit operates at maximum power dissipation. When VBUS.VALUE is above REGEN.VOLTSHIGH, the regen control commands the maximum duty cycle that the circuit can sustain given power and heating conditions.
The drive recalculates REGEN.VOLTSHIGH when VBUS.ACNOMINAL changes (or VBUS.DCNOMINAL when VBUS.DCOPERATION = 1).
Examples
Usage
The drive configures the REGEN.VOLTSHIGH parameter based on power board ratings and the value of REGEN.VOLTSHIGH is automatically set when the value of VBUS.ACNOMINAL is changed.
| VBUS.ACNOMINAL | REGEN.VOLTSHIGH | |
|---|---|---|
| Medium Voltage (MV) | 240 | 400 |
| High Voltage (HV) | 480 | 800 |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-09-02-000 |
General Information
| Type | Read Only |
| Units | VDC |
| Range | N/A |
| Default Value | N/A |
| Data Type | Integer |
| See Also | VBUS.VALUE, REGEN.VOLTSLOW |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
REGEN.VOLTSHIGH |
3007h |
10h |
Unsigned16 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2415 |
1 |
2415 (0x96f) |
REGEN.VOLTSHIGH |
Unsigned16 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
REGEN.VOLTSHIGH |
2415 |
Unsigned16 |
Read Only |
- |